From the Display 1 or Display 2 tab, click the MultiList
button to create a new display view. Only one MultiList display view can be added per Power Meter application.

button (near the top of the Display tab) and select the desired measurements. 
On the right side of the current display view, a Tools Palette provides controls for the following display options.
|
Change the title at the top of the current display view. |
|
Reset the size of the displayed font for the MultiList view to its default value. |
|
Increase the size of the displayed font for the MultiList view. You can change the font size when measurements are running or stopped. |
|
Decrease the size of the displayed font for the MultiList view. You can change the font size when measurements are running or stopped. |
|
Add a mathematical operation to measurements in the current view. You can choose to assign more than one operation to the current view. |
|
Remove the selected mathematical operation from the current list. |
To add a mathematical operation to measurements in the current view, click
to open the "Math Builder" dialog. You can choose to assign more than one operation to the current view.
The following math operations are available:
To remove an existing mathematical operation, select the desired operation from the list and click
.
button next to the "Measurement" properties drop-down pane. Measurements and operations will be displayed in real time. To stop the measurement acquisition for this view, click the
button next to the "Measurement" properties drop-down pane.
button located at the bottom of the Settings tab. Measurements and operations will be displayed in real time. To stop all assigned measurements on all display views simultaneously, click the
button located at the bottom of the Settings tab.As shown in the screen capture above, an Information Panel drop-down is provided under the current display view. This panel summarizes important measurement information for the current display view.
For the MultiList view, the Information Panel provides a summary of Alert Limit conditions for the current measurement. For more information, see Set Measurement Alert Limits.